ACTION#.TASKPARAM

Description

Some tasks require a Task Param value to specify what is acted upon. ACTION#.TASK must be set before ACTION#.TASKPARAM. If ACTION#.TASK is modified, then the range and units of ACTION#.TASKPARAM may be modified, and the value will be defaulted.

Not all tasks require a task param.

Example

This example shows an action which starts a motion task 4 on AXIS1

>> ACTION1.TASK = 5 (Launch motion task)

>> ACTION1.TASKID = 1 (AXIS1)

>> ACTION1.TASKPARAM = 4

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.TASK

Default Value

Depends on ACTION#.TASK

Data Type

Float

Stored in Non Volatile Memory

Yes

Task Parameter values for certain tasks

Task: Set the Command Source and Op-Mode for an axis.

Command Source and Op-mode combination Value
Service/TorqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist 0
Service/Velocity 1
Service/Position 2
Service/No Change 9
FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design/Torque 10
Fieldbus/Velocity 11
Fieldbus/Position 12
Fieldbus/No Change 19
Electronic Gearing/Position 22
Analog/Torque 30
Analog/Velocity 31
Analog/Position 32
Analog/No Change 39
No Change/Torque 90
No Change/Velocity 91
No Change/Position 92

Variants Supported

All variants are supported.